|
When Leuze electronic introduced the world's first laser barcode positioning system BPS years ago, the market was excited by the new possibilities opened by these systems. Precise position determination independent of reference points facilitates the detection of absolute position in every situation. With this and many other features, the Leuze electronic BPS quickly became the industry standard and is today an essential part of modern automation.
Reliability has a name BPS
With resolution down to the hundredth of a millimeter, our currently 15,000 installed BPS devices provide detailed information from more than 700 kilometers of laid barcode tape. In practical use, the laser-based devices perform dependably under a wide range of environmental conditions and also offer high dynamics and reading reliability through industry-tested laser technology.
  |
|

|
|
Dr. Konrad Kern,
EISENMANN AG:
"We have used the compact and stable Leuze BPS system for quite some time in our facilities. This has, in particular, been beneficial to the high availability of our systems." |
|
| BPS 8 |
|
BPS 34 / 37 |
|
|
|
|
|
|
|
|
Superior technology from the specialists for laser sensors
The mature laser technology, which Leuze electronic has also successfully employed in hundreds of thousands of other sensor systems, gives the BPS devices decisive advantages.
The most important features at a glance.
- The world's only barcode detection system that performs at speeds of up to 10 m/s enables a more efficient work cycle
- Tolerances, which are, by far, the greatest on the market with respect to reading angle, reading depth and deviations during travel around curves, serve to prevent system failures
- Long laser service life through robust laser diodes and optimized laser power regulation
- Highly flexible, self-adhesive plastic barcode tape with extremely high abrasion resistance as well as resistance against UV light, humidity and chemicals
|