The new HRTR 46B-TEACH enables configuration and diagnostics directly from the control, thereby saving a lot of time.
The times of long distances between the system control and the sensor are now a thing of the past thanks to the newest IO-Link sensor. Thanks to the possibility of configuring and diagnosing the sensor directly in the system control, not only is the start-up of a system considerably accelerated, but restoring a setting after replacing the sensor is child's play. In addition, these sensors also increase the flexibility of a system, since, for example, formats can be converted quickly and automatically.
Buy one sensor and get the performance of two - that's what we call efficient!
With the new HRTR 46B-TEACH, two sensors are integrated into one housing. With the newly-developed, site-sensitive sensor, the devices return two independent switching signals, depending on the model. This makes it possible to realize complex tasks such as two point regulations with only one sensor.
|
|

 |