News


Inner values are what really matter



A world's first PROFINET inside

For a relationship to function, inner values are much more important than trendy external appearances. And this applies not only to people. Our barcode readers of the BCL 500i series, for example, convince primarily with their suitability for practical use and the large bandwidth at integrated fieldbus interfaces. Brand new here is our BCL 548i, the world's first device with an integrated PROFINET interface, which considerably simplifies handling.

more...



We congratulate on the 700 millionth millimeter.



We congratulate on the 700 millionth millimeter.

When Leuze electronic introduced the world's first laser barcode positioning system BPS years ago, the market was excited by the new possibilities opened by these systems. Precise position determination independent of reference points facilitates the detection of absolute position in every situation.

more...



Everybody's Darling



Machines would buy Leuze electronic!

What would happen if, tomorrow, applications themselves could decide with which components they wish to be equipped? Our money would be on Leuze electronic. What more can an industrial robot wish for than components that make error-free and reliable operation possible and, for example, in the area of handling technology and robotics, ensure that the efficiency and reliability of a system increase?

more...



This family can truly deliver.



Our contrast scanner family convinces in all disciplines.

The use of contrast scanners in packaging and automation technology, e.g. for the detection of print marks, is commonplace today. For this application, we offer with our KRT 20B a scanner that, depending on features, can simply replace many competitor products with respect to technology and mounting, and do so with an unbeatable price/performance ratio.

more...



New sales catalogues



New sales catalogues

Request yours now.

more...



Can you see the light?



The LSIS 400i series.
Smart camera of the next generation.

The smart cameras score points compared to more complex systems in particular when it's about fast and low-cost integration. The flexible and high-performance systems of the LSIS 400i series are therefore the right choice for many automation applications.

more...



Master of all classes.



The new ODSL 9.

The best of the affordable. The most affordable of the best.

There's not much more to say when it comes to describing our new ODSL 9 optical distance sensors. With their very attractive price, the sensors open entirely new possibilities, even in demanding applications.

more...



get closer = highest productivity



The new GS 61 and GS 63 optical forked photoelectric sensors:
more flexible – faster – more reliable

Series GS 61 and GS 63, with their slim-line design and considerably reduced fork height, can be very flexibly integrated, e.g. directly at the front on the dispensing edge of a system.

more...



Interested in something new?



Practical solutions

Innovative products for intralogistics, packaging technology and electonics / robotics

more...



Can you read two things at once?



The LSIS 120 scans both barcodes and 2D codes in one device.

The reading of barcodes and 2D codes usually requires different systems: the classic scanner for barcode reading and the camera for 2D codes. These times are gone now for handling and testing machines, robotic systems and analytic automation.

more...



How safely do you switch off hazards?



The simplest and best option are Safety Switches and Safety Locking Devices by Leuze electronic.

Our diverse product range not only includes switches with separate actuators, but also Safety Hinge Switches and Safety Position Switches.

more...



More range opens up completely new possibilities.



The RS4-6E Safety Laser Scanner has an “eye on everything” with up to 6.25 meters.

The new flagship of the ROTOSCAN RS4 Laser Scanner family – just like all other members – provides reliability, flexibility and easy handling to make your processes safe and sound.

more...



When your plant can't quite cut it.



Availability is our strength.

Other than mere sensor technology, optimal alignment is also highly instrumental in ensuring plant reliability and availability. Here our proven throughbeam photoelectric sensors with brightVision® technology score in combination with the new SAT 5 Sensorscope twofold. These cannot practically be surpassed in terms of availablity and efficiency, even under adverse environmental conditions.

more...



Some people can't even get one thing right!



The new RS4-4M Safety Laser Scanner can take care of two tasks at once – no problem.

All the members of our ROTOSCAN RS4 family flawlessly complete their protection task as flexible multitalents for people safety. Our customers know this – as do many others. But the new ROTOSCAN RS4-4M Safety Laser Scanner can do even more.

more...



And, how’s your tolerance threshold?



And, how’s your tolerance threshold?

This innovation can automatically adjust its own threshold! Our ultrasonic forked sensors of the IGSU 14B series utilise the unique ALC technology for reliable detection, even if the label material has imperfections.

more...



Some things just are easier than they look...



... Safety at Work with AS-i solutions from Leuze electronic for example.

With our AS-i Safety at Work technology for the intelligent and efficient use of Leuze electronic Safety Sensors with integrated AS-i Interface, implementing AS-i-based Safety Sensor technology just gets so much easier for you!

more...



intelligent, outgoing, flexibel looking for ...



… a wide variety field buses for uncomplicated collaboration.

The Barcode reader of the BCL 500i series set new standards in connectivity.

All-in-all, a super find. Convince yourself.

more...



IO-Link - Breakthrough in communication technology



IO-Link - Breakthrough in communication technology

Sensors and actuators on the lowest operating level have long since been invested with their own intelligence and with the ability to supply wide-ranging types of information. But despite the diversity of available configurations and interface technologies, what has been missing to date has been an economical solution to address the issue of continuous communication right down to the lowest field level.

more...



Comparison between data matrix and bar code



Comparison between data matrix and bar code

The "data matrix code" is probably the best known member of the 2D code family and is frequently used for permanent direct labelling on, for example, tools, engine and motor components, and surgical/medical instruments. The data matrix code is also increasingly being used in production, vehicle manufacturing, chemical and biomedical analysis instruments as well as document handling.

more...



ATEX - Ex-Protection

ATEX - Ex-Protection

Since 1 July 2003, all devices and protective systems that are to be used in situations where there is risk of an explosion must conform to the new Directive 94/9/EC (ATEX 95). On the basis of this Directive, the European Community has formulated consistent and universally binding requirements for product quality, installation and maintenance with reference to the protection of systems, devices and components against explosion.

more...