|
The functions of the 3B compact series from Leuze electronic have been extended to include the HRTR 3B-V and HRTL 3B reflection light scanners.
|
|
 |
In the 3B series from Leuze electronic, users will find the smallest reflection light scanners of this performance class with the widest range of functions in relation to the sensor size. It also includes versions HRTR 3B-V and HRTL 3B. Both are reflection light scanners with background suppression. The V in the designation of the new HRTR 3B-V sensors stands for so-called "V optics" that permit the detection of glossy, reflective or transparent objects.
Also for the first time in this compact design, Leuze electronic is offering the HRTL 3B laser scanners in both laser class 1 and 2, each with excellent scanning range limits of 400 or 500 mm. One special feature is the collimated light beam that allows the HRTL 3B laser scanners to be universally used with a practically constant switching behavior over the whole scanning area.
|