|
|
|
|
The reading of quickly moving labels is a big and frequent challenge encountered by smart cameras in practical applications. The new LSIS 422i from Leuze electronic reliably masters this task and offers all of the advantages of the LSIS 400 series, such as the practical Web-based configuration with a standard browser.
|
|
 |
The LSIS 422i smart camera simultaneously reads up to 99 2D Data Matrix codes or barcodes on each image. As a result, it can be used anywhere various labels need to be detected and evaluated at high speed. Both the very short exposure time of just 54 µs as well as the device software contribute decisively to the performance. The user can, for example, read even inverse 2D codes. He can also adjust the sensitivity to the given application and specify quality criteria that must be maintained. In this way, the LSIS 422i smart camera ensures not only high reading speed, but also a high level of reliability.
|