Press releases 2008

Safety Sensors, Safety Systems, Safety Services




High protective field ranges up to 6 meters
In addition to the ROTOSCAN RS4-4M device variants already presented this spring, which boast the new MotionMonitoring function, the growing Leuze electronic Safety Laser Scanner family now also features the ROTOSCAN RS4-6E and RS4-6M variants with a protective field range of up to 6.25 m. These new highlights are equipped with both the “Extended” function package for danger zone and access guarding, and the “MotionMonitoring” function package for transfer trolley operation.
more...

Safexpert 6.0 – taking you to state-of-the-art standardization
EN 1050, the (by now) rather familiar harmonized standard for risk assessment, has been replaced by EN ISO 14121-1. This means that the users of all hazard lists created in accordance with EN 1050 must now change or even create these lists again. The new version 6.0 of Leuze electronic’s Safexpert Safet Engineering Software already includes the hazard lists in accordance with EN ISO 14121-1.
more...

Safety Sensors keep goal!
GOALIAS – that’s the name of the latest innovation project at the IAS, the Institute for Automation and Software Engineering at the University of Stuttgart. Leuze electronic participated in this project as a cooperation and development partner for the necessary opto-electronic safety sensor technology
more...

Safety Light Curtain with shape scanning
The new COMPACTplus-XSS/R Safety Light Curtains (XSS: eXtended Shape Scanning) are used with roll printing processes. They guard the access area when feeding in rectangular objects, such as paper rolls in the print and paper industry, for example.
more...

Safety at sheet delivery areas of sheet-fed printing machines
The sheet delivery of sheet-fed printing machines is the work station where the printed sheets of paper are automatically laid on a palette. In this area the operator must be able to reach in to move palettes in and out, remove print tests or insert pile wedges.
more...

Cascadable Type 4 Safety Light Curtains
SOLID-4E Safety Light Curtains can be used both vertical as hand protection, finger protection or access guarding, or horizontal for danger zone guarding. Cascaded devices allow these applications to be easily combined with one another. Both fixed connections in L-shape and U-shape versions and variants with flexible cable connections can be used here.
more...

Reliable protection on paper-cutting machines
The blade and paper-holding components in cutting machines are danger points that must be reliably guarded to protect the operator. A good solution to protect the operator from injuries when working on the machine is provided by the SOLID-4cutter, a type 4 Safety Light Curtain in accordance with IEC/EN 61496 that complies with the specifications of EN 1010-3.
more...

ROTOSCAN RS4-4M with new functions for operation on transfer trolleys
Leuze electronic will present its flexible multitalent for people safety with the new function extension "Motion" for the first time at the Hanover Trade Fair 2008. Intelligent sensors boast the ability (among others) to perform several tasks at one time. A task can therefore generally be completed quicker and easier – and the user saves money. The new ROTOSCAN RS4-4M Safety Laser Scanner is a good example of this type of function integration..
more...

AS-i Safety Monitor with Muting functions
The ASM2E AS-i Safety Monitor was successfully launched this year. The Muting function long awaited by the market and users alike, has now been added to the E-variants of Leuze electronic’s ASM Safety Monitors.
more...

New PC software for safety engineering
The SiSteMa safety engineering software is provided to the user as freeware by BGIA (German Institute for Occupational Health and Safety). Leuze electronic has supplemented the software with a manufacturer-specific database with all the safety-related parameters of selected Leuze safety sensors and control modules that SisteMa requires.
more...

Safexpert Version 5.5
Safety officers must know about changes in the world of standards. This is why the Safexpert Version 5.5 now includes a NormManager (standards manager), which immediately presents changes in the Official EU Journal (with regard, for example, to EN ISO 13849-1). Gone are the days when users regularly received CD ROMs with updates and had to do laborious research work.
more...