| 11.12.2007 |
Good reasons to take a closer look |
Sensors from Leuze electronic are renowned for extraordinary performance. A new generation of sensors has now been launched which encompasses a variety of standard series. Technological advances and new production techniques offer maximum functional reliability and handling convenience coupled with an optimum cost-to-performance ratio.
more
|
| 05.09.2007 |
Mini technology brings maxi benefits |
With its 3B series, Leuze electronic is offering a whole new generation of miniature-format diffuse reflection light scanners. Alongside wide scanning ranges and improved performance reserves, characteristic technologies of the series include external and spurious light source suppression and brightVision®.
more
|
| 05.09.2007 |
The fascinating world of the bar code |
The use of bar codes and suitable bar code reading systems can open up scope for the simple automation and optimization of operating processes. With the aid of the world's smallest bar code reader, this technology can be used even in miniaturized systems and devices or wherever space is at a premium. The BCL 8 is the size of a matchbox, making it ideal for solutions under even the most cramped conditions.
more
|
| 02.07.2007 |
Series 46B diffuse reflection light scanner sets whole new standards. |
The new series 46B reflection light scanners from Leuze electronic offer considerably greater performance reserves and ranges coupled with an increased setting range. High-speed commissioning with the aid of brightVision® and Ultra-Lock™, reliable detection of wide-ranging different objects and a long service life even under adverse environmental conditions guarantee low costs over the entire life cycle of the product.
more
|
| 02.07.2007 |
Bar code reader series BCL 31/32/34 for greater vision! |
The proven bar code reader series BCL 3x has just got even better, benefiting from a number of innovative production technologies and on-going technological development. One new feature is the F lens, a special lens permitting greater ranges of up to 100 mm (module-dependent).
more
|
| 02.07.2007 |
Making the most of the "white stuff" with Leuze RFID |
Milk producers have been highly creative in boosting product awareness over the years, capturing the attention of the public with a range of catchy slogans. Last year one of Germany's major national milk producers, NORDMILCH AG, faced one of its toughest challenges yet: To optimize its milk registration and acceptance processes.
more
|
| 11.04.2007 |
Product-News on hanover fair 2007 |
Focusing on market demand and the needs of our customers, we work continuously to engineer innovative, practically oriented systems based on state-of-the-art technology. Speed, precision, reliability, handling simplicity and top connectivity are the foundation stones on which Leuze electronic systems are developed.
|
|
People give Leuze electronic its brand personality |
|
Alongside the rich fund of expertise that has evolved over the past 40 years in the field of optoelectronic sensors within the Leuze electronic Group, it is the personal commitment and an actively implemented philosophy of customer orientation which have turned Leuze electronic into a brand with an unmistakable personality of its own. This unique people-based approach is expressed by the company’s new slogan “the sensor people”, which epitomises everything that makes Leuze what it is today.
more
|
|
Next-generation barcode reader with integrated connectivity |
|
The Leuze electronic barcode reader family has just been increased to include the BCL 500/i, a new product series featuring a range of more sophisticated performance features. An adjustable scanning rate of 800 to 1200 scans per second and a reading field of 200 by 1600 millimetres places the new models in the category of high-speed scanners for extremely fast processes. Special features of the series include code reconstruction technology (CRT) and integrated field bus connectivity.
more
|
|
Optical distance sensors supply data in two millisecond cycle. |
|
With its ODS 96B, Leuze electronic is launching a new generation of optical distance sensors designed to permit the detection of highly dynamic processes by performing unusually high-frequency measurements.
more
|
|
First area scanning distance sensors to feature Fast Ethernet |
|
Area scanning distance sensors (ROD 4) from Leuze electronic supply 2D depth information with a pick-up angle of 190°, so permitting the width, contour and position of an object to be detected. The new ROD 4plus is the first of its performance class to feature integrated Fast Ethernet.
more
|
|
Direct software start via TCI - Tool Calling Interface (TCI) for the RS4soft and SafetyLab graphic user interfaces |
|
The integration of field devices as slaves on PROFIBUS-DP and PROFINET-IO is generally made using the device-specific GSD file. This is interpreted by an engineering system, such as STEP 7 from Siemens, and provides the user with a user interface for setting device parameters. However the GSD file is not suitable when safety-relevant or many and complex parameters have to be set
more...
|
|
To some it’s just a plug for you it’s the easiest way to configure your safety laser scanner! |
|
The latest generation of Leuze Safety Laser Scanners: ROTOSCAN RS4 with intelligent ConfigPlug for easiest device exchange with no configuration expense
more...
|
| 26.01.2007 |
Environmental protection is integral to the Leuze electronic Group corporate standard (Leu 458) |
|
|
The company Leuze electronic has always stood for a responsible approach to environmental conservation. With its certification to DIN EN ISO 14001, the company has now provided further concrete proof of its exemplary standing on the environment.
more...
|
| 24.01.2007 |
Leuze electronic sensors qualified to ECOLAB standard (Leu 455) |
|
|
Certified to ECOLAB and IP 69K standards, optoelectronic sensors from Leuze offer outstanding seal protection and material resistance in compliance with the extreme demands made on modern industrial systems, particularly in the food and pharmaceutical sectors. To comply with ECOLAB standards, Leuze has extended its testing schedule to include additional substances under more severe operating conditions.
more...
|