| Switching light-section sensor – now with integrated PROFIBUS-DP |
Efficient data exchange via PROFIBUS-DP expands the functionality of the LRS switching light-section sensor from Leuze electronic. In up to 16 detection windows with logical linking option, up to 16 inspection tasks can be processed simultaneously in 10 millisecond cycles.
more
|
| Fieldbus connectivity for optical distance sensors |
New interface cables and modular interfacing units from the MA 200i family now facilitate the integration of optical distance sensors from Leuze electronic into Ethernet and fieldbus environments.
more
|
| New compact sensor for precise distance measurement up to 650 mm |
With the ODSL 9 series, Leuze electronic has extended its family of optical distance sensors and set new benchmarks for range, precision, compact design and comfortable operation.
more
|
| Coded magnetic safety systems |
With coded magnetic sensors and evaluation units, Leuze electronic offers special safety systems for extremely rough environments.
more
|
| Programmed for safety |
The new MSI 100 programmable Safety Controllers – with 20 safe inputs – control machines with a wide range of different safety components, including E-STOP buttons, two-hand controls, Safety Switches, locking devices or light barriers. In addition, the compact Safety Controller, just 67.5 mm wide, can monitor up to four drive components independent of one another.
more
|
| New functions in the 3B sensor series |
The functions of the 3B compact series from Leuze electronic have been extended to include the HRTR 3B-V and HRTL 3B reflection light scanners.
more
|
| Inductive switches in new cubic designs |
The new IS 240 and IS 244 sensor variants from Leuze electronic impress in particular with their wide scanning ranges and very simple mounting and alignment.
more
|
| The general trend with code readers doesn't stop short of hand-held scanners |
In spite of newer technologies, e.g. RFID, the use of barcodes and 2D codes for material flow applications has not fallen off.
more
|
| Optimal light spots for every application |
Leuze electronic has designed the new HRTR 25B-S reflection light scanner with focussed light spot optimally for the detection of glossy surfaces – and equipped the HRTR 25B-XL scanner with an extra large light spot for positioning tasks at the same time.
more
|
| Unlimited laser distance measurements |
The new laser distance measurement systems AMS 300i offer a previously unmatched selection of integrated interfaces.
more
|
| Further RFID products, now also in the UHF range |
Leuze electronic, the specialist for industrial identification technology, is extending its RFID product range to include additional stationary and mobile read/write systems which, thanks to the UHF range, are predestined for intralogistics applications.
more
|
| Muting accessories for light barriers |
With the new Muting Sensor Sets for the MLD Multiple Light Beam Safety Devices from Leuze electronic, muting solutions can now be implemented in an even quicker and easier manner.
more
|
| Reading of Pharmacodes now possible |
In addition to Data Matrix codes and the most important 1D barcodes, the new device software now enables the reading of Pharmacodes for the LSIS 400i Smart Camera from Leuze electronic.
more
|
| The newest generation of IO-Link sensors |
With the HRTR 46B TEACH, Leuze electronic has developed a new sensor which enables electronic adjustment via teach in and IO-Link and thus configuration and diagnostics in the process.
more
|