Press releases & contact

Basics for journalists – quick and professional

In this area, a plethora of current and general information is provided for journalists and editors. You can also sign up for our press distribution list!

04-Dec-2015

Reading Bar Codes in the High-End Sector

For the reading of 1D bar codes, one would have a hard time finding a scanner on the market today that is more powerful than the BCL 900i. More...
20-Nov-2015

Safety Locking Devices with RFID

New in the product line from Leuze electronic are the L300 safety locking devices, which are based on RFID technology. More...
06-Nov-2015

High-end safety laser scanner

Leuze electronic rounds off its new safety laser scanner series with device model RSL 440. More...
03-Nov-2015

All-in-one measurement station

The LSC 200 is a complete system for applications in intralogistics and packaging systems in which sensors and evaluation unit are optimally matched to one another. More...
28-Oct-2015

Vibration Resistant for Presses

Special V-models of the MLC 500 series safety light curtains have been opti-mized explicitly for applications subject to strong vibrations, such as for safe-guarding presses and punching machines. More...
22-Oct-2015

Tolerant Distance Sensors

The 10 series will win you over above all with their high tolerance to different materials. More...
28-Sep-2015

Hand-held scanner for all operating ranges

With new mobile code readers, Leuze electronic offers solutions tailored to cover all desired reading ranges. More...
28-Sep-2015

Sensors and signal lamps from one source

Leuze electronic now offers a versatile range of industrial LED signal lamps with degree of protection IP 66 for a temperature range of -30°C to 60°C. More...
01-Sep-2015

CCD scanners from mini to maxi

Leuze electronic not only provides readers for logistics applications, it also offers readers for special tasks – and the variety of readers is growing, for example in the case of miniature scanners for the automation of laboratory analyses. More...
10-Aug-2015

Line of inductive switches expanded

Leuze electronic has expanded its line of inductive switches and, as a result, now has a well-matched line of sensors for its core industries, such as intralogistics, packaging systems, the wood products industry, robotics and tool manufacturing. More...
08-Jul-2015

Purchase sensors at the click of the mouse

In the new Leuze electronic webshop, the choice of sensors is large and purchasing is simple. More...
03-Jul-2015

New sensor family for demanding tasks

Photoelectric sensors and light scanners of the SR 46C series impress with increased function reserve More...
20-May-2015

Switching light curtains for fast processes

The deep-freeze suitable light curtains from Leuze electronic for detection are faster than ever. Very short cycle times of 30 µs per beam reliably detect even fast processes. In addition, small, application-optimized CSR 780 devices are now also available with functionality based on the reflection principle. More...
04-Mar-2015

All-rounder with large operating range

Leuze electronic has trimmed the new SR 49C series for performance and flexible use in various fields of application. More...
02-Mar-2015

Bar code reader with blue light

The new BCL 600i product line from Leuze electronic operates with blue laser light and achieves astonishing read results with it. More...
28-Feb-2015

Safety with new photoelectric sensor

The new SLS 46C single beam safety devices can be used both as type 4 as well as type 2 sensors. More...
02-Feb-2015

Easy handling with address link label

The commissioning of all Leuze electronic products which have an Ethernet interface available, such as Profinet, has now been simplified even further – by means of a sticker with a MAC address, a so-called "address link label". More...
28-Jan-2015

Setting the bar high

RSL 400 – the new safety laser scanner series from Leuze electronic More...
26-Jan-2015

Proceeds donated

Leuze electronic supports the Brückenhaus e. V. in Kirchheim unter Teck with 2,500 euros. More...
18-Dec-2014

A wonderful idea

Trainees and students at Leuze electronic hold a charity Christmas market this winter More...
18-Nov-2014

Restructuring of Leuze electronic in Australia

The foundation of Leuze electronic Pty Ltd Australia/New Zealand on 1st Juli 2014 will strengthen the sensor manufacturer's position "down under". More...
04-Nov-2014

Extended range of EX sensors

CML 700i measuring light curtains and MLC 500 type 4 safety light curtains can now be used as EX versions for special applications in potentially explosive areas. More...
30-Oct-2014

Transmit data interference-free with light

With the DDLS 500, Leuze electronic has developed a data transmission photoelectric sensor that, in addition to a high transmission rate of 100 Mbit/s, sets new standards – above all with respect to usability. More...
22-Oct-2014

MLC now with integrated AS-i interface

The safety light curtains of the MLC series are now also available with an integrated AS-i Safety interface. More...
01-Oct-2014

BPS 300i with large range of bus interfaces

With the addition of the Profibus and SSI interfaces, Leuze electronic further expands its new BPS 300i bar code positioning system in the area of connectivity. More...
25-Sep-2014

Basketball in the sensor technology center

At the start of the new season of Germany's second division basketball league, the Kirchheim Knights appeared in the lobby of the team's main sponsor, Leuze electronic. More...
28-Aug-2014

Cascadable Type 4 Safety Light Curtains

MLC 500 safety light curtains are now also available as linked versions. More...
04-Aug-2014

Guarding with Stainless Steel

S420 is the name of the new stainless-steel safety hinge switch with which Leuze electronic optimally solves mechanically and hygienically challenging problems. More...
07-Jul-2014

Pluggable relay module for safety controllers

With the new MSI-EM-4RO relay extension module for the MSI 200 safety controller, users can control multiple devices via potential-free output contacts. More...
02-Jul-2014

Bar code reader for medicine

The CR 50 is a miniaturized, economical CCD scanner – specially designed for optimum integration in medical instruments for automating bar code readings in analysis technology. More...
28-May-2014

Lots of news and prominent visit to Leuze electronic

On the very first day of the CeMAT trade fair on 19 May, Leuze electronic GmbH + Co. KG, based in Owen (Germany), welcomed a high class visit to our booth at the world's most important exhibition for the intralogistics sector. More...
06-May-2014

Teaching via display

The LRS 36 switching light section sensor from Leuze electronic can now be conveniently taught directly on the device with a new teach function. More...
10-Mar-2014

Now with IO-Link interface

The LV463 fiber optic amplifier has been equipped with an IO-Link interface. More...
05-Mar-2014

The new BPS is here!

Leuze electronic invented the BPS bar code positioning system more than 10 years ago. The second generation of these established devices is now available in the new Leuze electronic product design. More...
26-Feb-2014

Safety light curtains in a practical set

Leuze electronic has expanded its successful product range of protective sensor sets with models MLC-UDC and MLCSET with safety light curtains. More...
03-Feb-2014

Risk assessments and CE certification from the professionals

Safety Consulting is the new service offering from Leuze electronic. It rounds out the Machine Safety Services portfolio – a comprehensive package consisting of services and support focused on machine safety. More...
23-Dec-2013

Basketball Tournament for a Good Cause

Leuze electronic donates €1,000 to the Arbeitsgemeinschaft Hospiz Kirchheim/Teck. More...
19-Nov-2013

Two New Ultrasonic Sensors for switching and measuring

Fully metal-enclosed ultrasonic sensors with degree of protection IP 67, longer operating ranges and thus broader areas of application expand the Leuze electronic line of ultrasonic sensors. More...
19-Nov-2013

In Asia for Asia!

Successful start of production in China: Leuze electronic assembly opens plant in Shenzhen/Baimang with more than 100 invited guests. More...
13-Nov-2013

Safety Light Curtains for the Automotive Industry

With the new MLC 511 (SIL 3, PL e) and MLC 311 (SIL 1, PL c) safety light curtains, Leuze electronic responds to the specifications of AIDA with regard to the pin assignments of the sensor modules and connection cables. More...
06-Nov-2013

New Sensor Series 18B

With the 18B sensor series, Leuze electronic expands its extensive line of sensors in the area of high-performance sensors for transparent media. More...
04-Nov-2013

Bar code reader with Ethernet/IP interface

The BCL 358i modular bar code reader series from Leuze electronic has been expanded by another Ethernet-based device model with integrated Ethernet/IP interface. More...
01-Nov-2013

Well-Rounded Safety Device Family

The MSI safety device family from Leuze electronic has been completely redesigned and equipped with pluggable terminal blocks. More...
30-Oct-2013

Measuring light curtain for low temperatures

The CML 700i measuring light curtains now offer the possibility of use down to low temperatures of -30°C in addition to the integrated Profibus interface. More...
02-Aug-2013

Latest generation of hand-held scanners

With the mobile scanner series IT 1910i and IT 1911i, Leuze electronic offers two new series which provide an as yet unrivaled level of reliability. More...
19-Jul-2013

Company jubilee with dedication of sensor technology center

Leuze electronic opens new sensor technology center at headquarters in Owen. The new building was solemnly dedicated at the anniversary celebration in July, at which the employees celebrated the company's 50th birthday. More...
28-Jun-2013

Extremely tough

Leuze electronic is releasing new cylindrical sensors for particularly difficult conditions. More...
26-Jun-2013

Sensors for everything and everywhere

Leuze electronic is currently pursuing its strategy of offering standard sensors for nearly any application at an unbeatable price-performance ratio. Three new series are proof that this is working. More...
12-Jun-2013

Also ideal for measurement tasks

The LSIS 462i smart camera is now equipped with a measurement function and is therefore a step closer to being a complete system. More...
26-Apr-2013

Depth of field with blue light

Leuze electronic is now using a blue laser in the BCL 20 bar code reader series and, with its light with a wavelength of 405 nm, is achieving astounding results regarding depth of field, operating range and code reading at very small modulus widths. More...
12-Apr-2013

Expanded Connectivity for Sensors

Within the MA 200i series, Leuze electronic now also offers modular interfacing units for DeviceNet, EtherNet/IP and CANopen connections. More...
22-Mar-2013

New safety transponders (RFID)

With the new RD800 safety transponders, Leuze electronic provides special safety systems with closed designs (IP67, IP69K) for extremely tough or challenging application cases. More...
13-Feb-2013

Universal and sturdy

MLC is the intelligent Safety Light Curtain from Leuze electronic. More...
01-Feb-2013

Functional extensions

The Multiple Light Beam Safety Devices of the MLD series, designed for efficiency right from the start by Leuze electronic, have now been equipped with new functions as part of a further development. More...
25-Jan-2013

High resolution for small part measurement

The LPS 36 light section sensors from Leuze electronic now offer resolution up to 0.1 mm, which makes them perfectly suited for the measurement of small parts. More...
01-Nov-2012

Extremely fast measuring light curtains

With the CML 720 series, Leuze electronic is launching a new generation of measuring light curtains onto the market. More...
26-Oct-2012

Powerful sensors – versatile application

The new photoelectric sensors of the 28 series from Leuze electronic are equipped with many technical highlights, but they are characterized in particular by a sophisticated mounting concept. More...
03-Oct-2012

Bar code reader with oscillating mirror

The new modular BCL 300i bar code reader series is extended with a device model with oscillating mirror. More...
02-Oct-2012

Compact sensors – optimal for tight installation spaces

With series 5, Leuze electronic has developed universal photoelectric sensors which are consistently aligned to make the integration of sensors as easy and flexible as possible. More...
20-Sep-2012

Universally applicable jack-of-all-trades

Leuze electronic expands its line of hand-held scanner products with the new HS 65x8 DPM series. This series features hand-held scanners for rapidly reading 1D- and 2D-codes, both printed as well as directly marked (DPM codes). More...
05-Sep-2012

Lots of fiber optics and new amplifier

The LV463 fiber optic amplifier is a new addition to the pro-duct range from Leuze electronic and a high-performance device that, together with the corresponding fiber optics, always shines when the task calls for reliable detection in constricted spaces. More...
26-Jul-2012

Honor for Leuze electronic

Leuze electronic is the preferred supplier at Uhlmann More...
16-Jul-2012

Expansion continues

Leuze electronic strengthens its commitment on the Asian market with new subsidiary in India More...
15-May-2012

More efficient protection with sets

Leuze electronic is offering perfectly matched MLDSET Light Beam Safety Device Sets based on a modular system. They enable the easy and efficient construction of the most common access guarding systems with muting. More...
02-May-2012

Smart camera LSIS 400i with new features

The device models and the current software version of the LSIS 400i smart camera from Leuze electronic have been expanded. From now on, devices with integrated IR or RGBW LED illumination as well as a model for C-mount lenses are also available. New features were added to the software. More...
01-May-2012

Small, fast and very clever – the new LSIS 220 code reader

The LSIS 220 compact series reads 1D-codes, stacked codes and 2D-codes – omnidirectional, both during standstill and in motion. And it also offers increased performance reserves. More...
31-Jan-2012

Install photoelectric sensors more efficiently

With the "omni-mount" from Leuze electronic, pho-toelectric sensors can be mounted and adjusted quicker and more easily. More...