Opciones de filtro
Seleccione diferentes filtros para limitar su selección.
-
Trust is good. Monitoring is better.
High-performance identification systems from Leuze electronic make possible quick and reliable component identification in quality assurance with simple integration into all current fieldbus systems. Highly modern safety solutions also protect the quality assurance employees when they have to intervene in running processes and remove parts to be checked. Thanks to our sensor solutions, faulty work pieces can be identified, registered and removed from the process during fully-automated procedures.
-
Casting and storing automated parts
Increasing automation in production and storage of cast parts also necessitates automated logistics and process monitoring. Special sensor solutions are used here, since casting molds, for instance, can only be durably identified via temperature-proof RFID transponders. Highly-dynamic transport on conveying belts or using cranes and robots is also monitored with active optoelectronic protective devices and is safeguarded just like the actual casting area.
-
So that it moves forward
Different work and processing steps have to mesh together in a way that prevents as many faults as possible in the various assembly steps of a power train. This is why powerful sensor solutions in the smallest designs from Leuze electronic are used for the mounting of motors, gears and axles. Today, the material of power train components is directly equipped with 2D-codes. Highly-developed code readers ensure that the right parts are mounted at the right place at the right time.
-
From a simple plate to a complex component
These days, press plants are almost completely automated and are controlled and monitored using fast, resistant sensors. The plates are transported directly from the coils to the press line at whose end the completed punched and formed pieces are removed by robots. Modern manufacturing methods require the identification of plates, usually with dot-peened 2D-codes, to facilitate the monitoring of the further process sequence with code readers.
-
Extreme strain at the highest precision
In body shell production, different body types are often produced on one welding line. This type of flexibility requires faster and highly-precise sensors, e.g. for use in fitting tools. In addition, the sensors used are also exposed to extreme mechanical stress due to flying welding sparks and regular cleanings with dry ice. Leuze electronic has developed solutions to meet these demands.
-
Efficient corrosion protection and aesthetic paint jobs
At the latest during the elaborate catalytic dip coating process, the vehicle bodies or skids have to be marked using RFID transponders, since these are the only ones that sustainably withstand the immersion baths and oven drying at up to 200 °C. During the subsequent painting job with robots, powerful sensors and camera systems are also essential to ensure problem-free processes and consistent results.
-
From individual parts to a fully-functional vehicle
In the final mounting stage of a vehicle, man and machine work together very closely. Hazards must therefore be ruled out with reliable safety sensors. Furthermore, high quality standards require the consistent checking and logging of components marked with bar codes, 2D-codes or RFID. Leuze electronic has sensor systems suitable for detecting the location of the vehicle body on pushing platforms, skids or telpher lines at any time and checking its production status.
Aplicación | Área | Tarea |
---|---|---|
Component identification for facilitating traceability | Quality assurance | Bar code, 2D-code |
Guarding of manual workplaces | Quality assurance | Danger area safeguarding |
Identifying components during rework | Quality assurance | Bar code, 2D-code |
Cast-part testing | Foundry | Quality control |
Press mould identification in the foundry | Foundry | RFID, Presence inspection, Point of operation guarding |
Detection of shelf positions | Foundry | Positioning |
Work piece handling | Foundry | Danger area safeguarding |
Guarding of loading and unloading robots / portals | Powertrain | Danger area safeguarding, Access guarding |
Work piece identification in motor assembly | Powertrain | 2D-code |
Component identification in drive assembly | Powertrain | 2D-code |
Guarding of assembly workstations | Powertrain | Danger area safeguarding, Access guarding |
Sensors in axle assembly | Powertrain | Presence inspection, Distance, Orientation detection |
Direct work piece detection on mounting robot | Powertrain | Orientation detection |
Safeguarding and position determination on corridor supply vehicles | Powertrain | Positioning |
Component monitoring on corridor supply vehicles | Powertrain | Quality control |
Pick to light storage | Powertrain | Quality control |
Material handling | Powertrain | Presence inspection |
Positioning and communication on crane systems | Punching / reshaping technology | Optical data transmission, Positioning |
Press guarding | Punching / reshaping technology | Point of operation guarding |
Body shell material handling | Vehicle body shell | Positioning |
Guarding of welding robots | Vehicle body shell | Danger area safeguarding |
Sensors for welding robots | Vehicle body shell | Presence inspection, Orientation detection |
Gluing application on vehicle body sheets | Vehicle body shell | Dimension, contour, volume |
Sheet detection in vehicle body construction | Vehicle body shell | Presence inspection, Distance, Orientation detection |
Position detection on welding robots | Vehicle body shell | Positioning, Distance |
Pallet identification in vehicle body assembly | Vehicle body shell | Bar code, 2D-code |
Exact pallet positioning | Vehicle body shell | Presence inspection, Dimension, contour, volume |
Vehicle body detection | Paint finishing system | Machine protection / collision prevention |
Skid detection | Paint finishing system | RFID |
Painting booths | Paint finishing system | Danger area safeguarding |
Plug detection | Paint finishing system | Quality control, Dimension, contour, volume |
Positioning of sliding tables | Paint finishing system | Positioning |
Driver-less transportation system control | Final mounting | Positioning |
Pick and place | Final mounting | Orientation detection |
Vehicle body detection | Final mounting | RFID |
Object positioning | Final mounting | Presence inspection, Orientation detection, Quality control, Positioning |
Merge | Final mounting | Machine protection / collision prevention |
Guarding of assembly workstations | Final mounting | Danger area safeguarding |
Component identification in assembly | Final mounting | Quality control |
Position detection in factory automation / on telpher lines | Final mounting | Positioning |
Palette positioning | Final mounting | Positioning |