Data within a network is transferred in different ways. Optical data transmission photoelectric sensors use the ‘air’ medium to transfer data invisibly, contactlessly and wear-free over a distance of up to 300 m. This is a leading technology in plant engineering and combines efficiency with cost effectiveness.
Sensor solutions for primary packaging in beverage filling, pharmaceutical and meat packaging as well as confectionery and bakery production, for secondary packaging and for the end-of-line area.
Sensor solutions for hydraulic and eccentric presses, punching and laser cutting machines, pipe and wire bending machines, processing centers, hydraulic press brakes, metal sawing machines, sheet metal feeders and robot work areas.
Global industry is in a constant state of flux – and with it, the complex demands on safety systems designed to protect people and equipment. With a comprehensive portfolio to satisfy all safety requirements, we offer you complete safety, an efficient flow of materials, and maximum availability levels worldwide.
We are constantly working on technological challenges and important issues in the markets of our customers. This is a prerequisite for our efficient product development and consulting expertise.
Leuze is an international sensor expert for automation technology. With curiosity and determination, we – the Sensor People – have been forerunners for innovations and technological milestones in industrial automation for more than 60 years.
To us, innovation means using our curiosity and determination to the full extent in order to make you successful for the long-term in an ever changing industry. Your success is our objective and motivation.
We accompany our customers during the entire life cycle of their machines or systems by providing competent advice and offering our comprehensive support and services.
With over 20 subsidiaries and supported by more than 40 international distributors around the world, we are represented in the most important markets of our industry and are always in close proximity to our customers.
We are constantly working on challenges and important issues in the markets of our customers. This is what makes our consultation and development work so successful, enabling us to offer our customers efficient solutions.
Defective devices are repaired in our service center competently and quickly. We offer you an extensive service packet to keep any system downtimes to a minimum.
Leuze rounds off its laser scanner portfolio: The ROD 300 and ROD 500 series measuring laser scanners are complemented by the new ROD 100 series switching devices. These detect objects precisely and are ideally suited for collision protection tasks.
Ultra-compact, versatile, visionary: At SPS 2025, the Sensor People from Leuze will be presenting the smallest safety laser scanner on the market as well as other highlights for industrial automation (Hall 7A, Stand 230).
In industry, especially in warehouse logistics, a stable power supply is essential, as demonstrated by its importance in mobile applications like hand-held scanners. Supercapacitors (supercaps) provide energy storage solutions that intelligently complement conventional battery concepts. Leuze makes targeted use of the technology in its innovative sensor solutions.
New IT 1960 multi-purpose hand-held scanner series from Leuze: Supercap technology, up to 20 percent faster read processes, and higher contrast tolerance
In industrial automation, efficiency and safety must go hand in hand: People, machines and processes must be reliably protected without impairing production processes. However, space is limited in narrow production lines, on automated guided vehicles and robots. This is where the new ultra-compact RSL 200 safety laser scanner from Leuze scores points: As the smallest safety laser scanner on the market, it can be integrated effortlessly and used flexibly to safeguard danger zones and access points.
The LBK radar system from Leuze is now also available with a CIP safety interface. Persons in the danger zone are reliably detected by the 3D radar system from Leuze, even in harsh conditions – static objects do not lead to shutdown
The FBPS 600i safety bar code positioning system from Leuze is now also available with PROFIsafe interface. This makes safety features particularly easy to implement.
The new RFID readers for flexible use in production and logistics score points with their compact design, reading ranges of up to 100 mm, flexible mounting options and IO-Link.
LogiMAT 2025: Leuze presents the smallest safety laser scanner on the market
17 Feb 2025
| Press and public relations work
Visitors to LogiMAT in Stuttgart can look forward to innovative sensor highlights from Leuze – including the new ultra-compact RSL 200 safety laser scanner. The Leuze trade fair team will be on site from March 11 to 13: Hall 3, Booth C60.
Leuze presents the smallest safety laser scanner on the market
17 Feb 2025
| Press and public relations work
The new, ultra-compact RSL 200 safety laser scanner from Leuze safeguards machines, automated guided vehicles and robots. Thanks to its minimal dimensions, it is very easy to integrate even where space is limited.