Elektrohängebahn für den automatisierten Materialtransport

Sensor solutions for electrical monorail systems

Electrical monorail systems are rail-guided transport systems in which goods are transported from one station to the next on powered, suspended transport units. They must operate reliably on both straight and curved sections, position goods precisely, and ensure an efficient production process. Since multiple transport units often travel on the rails at the same time, reliable collision detection is of great importance. Suitable safety solutions are also required at transfer and working areas along the transportation path.

This transport system is used in particular for transporting hanging goods, for example in the textile industry or in large order-picking areas with a wide variety of items. In such settings, electric monorail systems enable an efficient and space-saving material flow.


Sensor technology on electrical monorail systems

Electrical monorail systems are used in large-scale production systems as well as in order-picking and distribution warehouses to efficiently transport load carriers and hanger goods. Precise positioning, reliable collision detection, and high system availability are crucial for smooth operation.

Suitable sensor solutions enable the exact positioning of transport units, ensure safe distances between vehicles, and safeguard transfer areas and dangerous areas. High-performance identification technologies such as bar codes, 2D-codes, and RFID also provide transparency and support efficient material flow processes.

Click on the numbered applications to learn more about the respective sensor solutions.


Applications on the electric monorail system

BPS Barcode-Positioniersystem zur präzisen Positionierung von Elektrohängebahnen in Distributionszentren.

Positioning of the transport unit

Requirement:

For control of the electric monorail system, the position of the transport unit on the carrier must be known with millimeter precision at all times.

Solution:

The compact BPS 8 and BPS 300i bar code positioning systems enable precise positioning over a length of up to 10,000 m. The devices can be easily integrated into the control thanks to a wide range of interfaces. The self-adhesive bar code tapes are optimized for industrial application and are extremely durable.

> Read more about positioning systems

FBPS Sicherheits-Barcode-Positioniersystem zur präzisen und sicheren Positionierung von Elektrohängebahnen in Distributionszentren.

Safe positioning of the transport unit

Requirement:

For control of the electric monorail system, the position of the transport unit on the carrier must be known with millimeter precision at all times. “Safe positioning” must be ensured especially when workers are working very close to the transport unit.

Solution:

The safe FBPS 600i bar code positioning systems enable precise positioning over a length of up to 10,000 m. The devices can be easily integrated into the control thanks to a wide range of interfaces. The self-adhesive bar code tapes are optimized for industrial application and are extremely durable.

Lichttaster zur Auffahrsicherung und Kollisionsvermeidung an Elektrohängebahnen in Distributionszentren.

Collision protection

Requirement:

When transporting goods by means of an electrical monorail system, collisions between the individual suspension gears should be avoided. For this purpose, the distance between the suspension gears must be determined.

Solution:

The ODS 10 optical distance sensors / HT 10 sensors with background suppression measure the distance between the suspension gears. The devices measure onto an any object or onto a cooperative reflector. They can be configured via the display or IO-Link.

ROD 100 Laserscanner zur Kollisionserkennung und Abstandsüberwachung an Elektrohängebahnen in Distributionszentren.

Collision detection

Requirement:

When transporting goods using an electric monorail system, collisions between units should be avoided. To do this, the distance between the vehicles must be monitored.

Solution:

The ROD 100 optical laser scanners detect when values fall below switching points within definable windows and send a switching signal to adjust distance and velocity.

Sicherheitsscanner zur Bereichssicherung von Lastabgabe- und Lastaufnahmebereichen an Elektrohängebahnen in Distributionszentren und der Fließfertigung.

Safeguarding the load pick-up and drop-off areas

Requirement:

The area where the goods are loaded or unloaded should be secured against access and presence of persons.

Solution:

The RSL 400 safety laser scanners secure even large areas with just one device thanks to their 270° scanning angle and up to 8.25 m operating range. Models with PROFIsafe / PROFINET interface enable easy integration into industrial networks and allow parallel monitoring of up to 4 protective fields.

Optische Code-Lesung zur zuverlässigen Identifikation von Paletten an Elektrohängebahnen in Distributionszentren.

Code reading on pallets

Requirement:

For control of the flow of goods, the goods code on the pallet must be read and transferred to the higher-level system.

Solution:

The BCL 500i / 600i series bar code readers read the codes on the pallets. Using the integrated switch, the devices can be connected both to each other and directly to the control system via a line structure. Different optics models also allow the devices to be optimally adapted to the reading task.

> Read more about laser-based 1D bar code readers


Jetzt Kontakt aufnehmen

Do you have questions about your electric monorail systems application?

Our team of experts will help you select the right sensor solution for your needs.


Frequently asked questions about electrical monorail systems

Electrical monorail systems are rail-guided transport systems in which goods are transported from one station to the next on powered, suspended transport units. They must be flexible and reliable on both straight and curved sections.

Since electrical monorail systems are typically operated in a continuous loop, absolute position determination is required. Various technical solutions are available for this, and the choice depends on criteria such as route length, travel speed, and the required interface. Track switches and their integration into the route must also be taken into account.

A particularly flexible and reliable solution is code-based positioning using a defined code tape, as enabled by the BPS (bar code positioning system). The large working range and reliable code detection make the system particularly suitable for applications involving curved paths.

The risk of a collision can be detected early using appropriate sensors, such as diffuse sensors. Depending on the application, the sensor signal can trigger an adjustment of the travel speed or the braking of the electric monorail.

Safety-critical areas are often located along the route, such as at loading and unloading points or at intersections with walkways. Before entering a transfer station, make sure that no one is in the dangerous areas. This requires reliable monitoring. Safety laser scanners with flexibly configurable protective fields are frequently used, enabling application-specific safeguarding.

For traceability, load carriers are often marked with codes that can also be used to control transport processes. These codes can often be detected and decoded as the load passes by the electric monorail system, enabling reliable identification without stopping.