Sensorlösungen für Verschieberegale in der Intralogistik.

Sensor solutions for side-tracking shelves in intralogistics

Automated intermediate warehouses and distribution centers often store goods that are only accessed occasionally. To make the most efficient use of costly storage space, automated movable shelving systems, known as side-tracking shelves, are used. Unlike fixed shelving systems, side-tracking shelves do not require permanent aisles between rows to be kept clear. The shelves are moved as needed, providing targeted access to the desired location. This allows for increased storage capacity within the same floor space.

Precise positioning of the shelves and employee safety are particularly crucial for safe and reliable operation. While the shelves are in motion, movements must be monitored and dangerous areas safeguarded to prevent collisions and ensure personal safety.


Sensor technology for side-tracking shelves

Side-tracking shelves enable space-saving and cost-effective storage by making optimal use of the available warehouse space. At the same time, individual rack areas must be quickly and safely accessible whenever required.

Sensor solutions from Leuze support the precise positioning and synchronized movement of the shelf and drive. In addition, single- and multi-beam safety sensors safeguard the foot space between shelf rows as well as the access points to the rack aisles. This ensures reliable movements and a high level of safety for employees.

Click on the numbered applications to learn more about the respective sensor solutions.


Applications for side-tracking shelves

SLS46C Einstrahl-Sicherheitssensor zur zuverlässigen Fußraumüberwachung an Verschieberegalen in der Lagertechnik.

Foot space monitoring

Requirement:

While the side-tracking shelf is moving, the foot space is to be monitored for the presence of persons. If multiple shelf rows are installed one behind the other, there must be no interference between the sensor signals of the rows.

Solution:

The SLS 46C single light beam safety devices monitor the foot space over a length of up to 70 m. They are available as a type 4 and a particularly easy-to-align type 2 variant. The use of models with red light and infrared light prevents mutual interference between the shelf rows.

Sensoren zur Auffahrsicherung und Abstandsüberwachung an Verschieberegalen für mehr Sicherheit und Kollisionsschutz in der Lagertechnik.

Collision protection and distance monitoring

Requirement:

When closing the aisle between two shelves, the shelves must be prevented from moving up. To do this, you need to determine the distance between the shelves. Two distances must be called up via switching outputs.

Solution:

The HT 46C series universal diffuse sensors use red or infrared light and work reliably even with dark and glossy objects. The devices have two switching outputs, each of which can be precisely taught to a distance.

> Read more about diffuse sensors with background suppression

MLD Mehrstrahl-Sicherheitslichtvorhang zur Zugangssicherung von Regalgängen an Verschieberegalen in der Lagertechnik.

Access guarding of the aisle

Requirement:

If a vehicle is in the aisle or the aisle is closed, access to this aisle must be secured.

Solution:

The multiple light beam optical safety sensors of the MLD 500 series are used for access guarding. For operating ranges up to 8 m, particularly cost-effective transceiver systems are available that require an electrical connection on only one side. Alternatively, transmitter-receiver systems offer operating ranges of up to 70 m.


Jetzt Kontakt aufnehmen

Are you looking for the right sensor solution for your side-tracking shelf system?

Our team of experts will help you select the right sensor solution for your needs.


Frequently asked questions about side-tracking shelves in intralogistics

To maximize the use of costly storage space in high-bay warehouses, automated mobile shelving systems, known as side-tracking shelves, can be installed where storage requirements justify their use.

The precise positioning of the racks, as well as the protection of the foot space and access areas during rack movement, are among the key sensor tasks in side-tracking shelf systems.

Optical safety sensors monitor both the foot space between the shelf rows – usually using single-beam safety light barriers – and the access areas to the rack aisles, where multi-beam safety light barriers are used. If people or body parts are detected in the monitored dangerous areas while the rack is moving, the movement is stopped to prevent injuries.

Diffuse sensors with background suppression detect when the rack approaches adjacent racks or reaches the end of its travel path. When the defined position is reached, a switching signal stops the drive to ensure precise positioning and prevent collisions.

When opening a rack aisle automatically, the passage width must be precisely adjusted for, e.g., industrial trucks. A position sensor enables repeatable rack positioning and ensures that the required clearance width is reliably achieved.