KI2_ret_1400x400px

Artificial Intelligence: Sensor Data for Increased Efficiency

Sensor data as the gateway to factory automation

Data is the key to success when it comes to intelligent production systems. Sensors generate large amounts of process data on a daily basis, and this data is transferred to the control system via a communication interface and processed. This data is already being used to manage systems and production lines and evaluate information, for more flexible processes and increased system availability.


 

Artificial intelligence provides the context

Artificial intelligence helps to make production processes more intelligent, flexible and economical by drawing on data generated from field components. AI algorithms evaluate large amounts of data and ascertain key performance indicators or actions that need to be taken so as to continuously improve system productivity. 

ki_bild_1

Artificial intelligence can be used, for example, to help differentiate various fault causes and quickly detect any nuisances. This especially pays off if there are multiple intelligent sensors installed in a system: When it comes to intralogistics, it’s possible for up to 1,000 bar code readers to be installed across distances that stretch for miles but are part of one system. Searching for the specific bar code reader that isn’t working properly can be as hard as searching for a needle in a haystack. Every bar code reader shares its status with an Ethernet-based Bus interface, for example: “Reading is precise” or “Reading is particularly poor”. Sensor data can be aggregated and context illustrated through an AI-supported evaluation process. Does the poor reading rate always occur on one bar code reader, only one label, with a certain type of label, or at a certain installation location? Nuisances can be quickly identified and rectified.

From the sensor to the cloud

Issues such as condition monitoring or predictive maintenance require sensors that are capable of making data available worldwide and in a standardized format. We have been a forerunner from the start, and we are working on standardizing industrial communication.

We offer sensors that deliver data, e.g. through IO-Link or via OPC UA, to the control or make it available to the cloud and edge devices. In this way, our smart sensors are capable of managing production processes and evaluating information so that any problems can be detected early on. 

ki_bild_2
2_IGRA_OPCUA_Automatisierungspyramide_Hierarchie_Netzwerk_DE

Our dual channel principle involves measurement data for process control being transferred in real time over the first channel, then the information for monitoring and analyzing the machine being transmitted over the second channel. The dual channel principle is also helpful in state monitoring and predictive maintenance during production. Soiling or misalignment of a sensor can change the signals to such an extent that switching faults occur. The dual channel principle can also assist commissioning. Based on the OPC UA communications standard, which has established itself as the standard protocol, the sensors transfer data into the cloud. Error messages can be sent to an operator this way and then resolved together. And this can be done on a global scale. OPC UA-certified sensors have been part of our range since as early as 2016.


Learn more

Using the IO-Link communication system, sensors and actuators can be integrated into a digital machine environment. Measurement data and other information can be prepared, such as device information or diagnostic data. This creates high process transparency, means sensor systems are easy to commission and makes preventative maintenance possible. As the founding member and technology developer of IO-Link, we possess extensive know-how. You always receive the latest technology – such as Smart Sensor Profile – and many sensors with additional functions as well as connection options to the cloud. With our networked solutions, you are prepared for the requirements of the smart factory.


Learn more

3_csm_leuze_io_link_header_1400x500px_095b283444_1600x1600

 

Leuze_GettyImages-900256746_edited_RGB_700x500px

Technologies

Industrial Ethernet, integrated connectivity and more kinds of technology: we are constantly working on technological challenges and important issues in the markets of our customers. 

Learn more