Technology report

Cyber Resilience Act: Greater security in industrial automation

The Cyber Resilience Act focuses on new requirements for digital, networked products. Find out how Leuze is making its sensor solutions ready for the future – and what customers need to know

In 2024, the EU enacted the Cyber Resilience Act (CRA (EU) 2024/2847), a cybersecurity regulation that will come into effect in phases: Starting September 11, 2026, manufacturers of products with digital elements will be required to report serious security incidents and actively exploited vulnerabilities to a central EU platform (Single Reporting Platform). In January 2027, the new Machinery Regulation (EU) 2023/1230 will take effect, setting specific requirements for cybersecurity and digital safety components. From December 2027, all new digital products placed on the market must be CRA-compliant. For manufacturers, this means they must assess and document cyber risks, establish a “Secure Development Life Cycle,” and may only bring products to market that are protected against cyberattacks in accordance with the current state of the art.

Cybersecurity for connected industrial systems

This is particularly important for industrial automation: In many industrial environments, legacy systems operate alongside modern digital systems. As machinery and control systems usually remain in use for many years, vulnerabilities can persist for a long time. At the same time, as connectivity increases, so does the attack surface. Even minor security vulnerabilities can result in production downtime or the loss of sensitive operational data. This is exactly where the CRA comes in: It is designed to ensure the security of devices with digital components – including many Leuze sensors – during development, operation, and throughout the entire product lifecycle. An important factor here is the ability to receive updates. The CRA requires that security updates be technically feasible and that manufacturers make them available as needed. Users thus benefit from products that are developed, operated, and supported in accordance with the latest security standards.

For which system components is the CRA relevant?

The CRA applies to all products with digitally networked components available on the EU market. These include networked hardware such as sensors and control systems, as well as software solutions in automated systems’ networks. The regulation requires manufacturers such as Leuze to conduct a systematic risk assessment to determine whether products are potentially vulnerable to cyberattacks. If risks are identified, countermeasures are taken. Proof of CRA compliance will be an integral part of the EU Declaration of Conformity in the future.

For newly developed sensors, the manufacturer guarantees through the EU Declaration of Conformity that they are protected against cyberattacks. When integrating sensors, machine builders must assess the risks to the entire system – similar to safety processes – and, if necessary, adapt their existing security concepts. Operators and integrators define a security level and the corresponding technical requirements, such as network segmentation with firewalls, user management, or logging systems. The sensors support this architecture to achieve the system’s defined security level. This provides end customers with machines that are reliable in the long term and resilient against attacks, production downtime, and the loss of sensitive data. Existing products that have already been installed in systems or are in storage do not necessarily need to be modified.

How manufacturers implement the requirements

Leuze began integrating the CRA’s requirements into its development and production processes at an early stage. The company’s many years of expertise in the field of safety – that is, workplace safety and personal protection – facilitated its expansion into security processes that ensure the protection of systems and networks against external attack scenarios. Both fields require comparable strategies and processes. The cornerstones of implementation are:

  • Security by design – digital products are developed in accordance with cybersecurity’s current state of the art. In the context of sensors, this specifically means that their architecture has been enhanced for security and includes, among other things, secure boot and file systems: Upon startup, the loaded software is validated and verified using security features on the device hardware. Data on the sensors is protected against tampering, and the system architecture enables encrypted data transmission over the sensors’ communication channels.
  • Security by default – the factory settings are designed to be cyber-secure by default, and all optional interfaces are disabled. Every user access must be authenticated. Sensors can be reset to factory settings at any time, and customer-specific data can be deleted.
  • Update capability – digital products in operation can be updated to the latest security standards. Where appropriate, updates are enabled via the process interface. If an update fails, the system reverts to the previous secure state.

How the CRA Is changing product development

Security considerations are incorporated into every phase of the development process for new sensors. This includes:

  • Systematic threat analysis: Leuze creates a risk matrix that examines and evaluates potential attack scenarios.
  • Minimizing attack surfaces: Strict security requirements are integrated right from the product development stage.
  • Providing security updates: Leuze defines lifecycles for the entire service life of its sensors. These lifecycles determine the duration of support and govern product succession. Leuze ensures that customers receive regular updates throughout the products’ planned service life. These updates ensure functionality and address identified vulnerabilities. In addition, mechanisms are being developed to enable the simultaneous updating of all Leuze products within a system.
  • Documentation Comprehensive documentation is created for each product to help customers use them safely.
  • Vulnerability management and reporting: Leuze has established processes to identify and manage vulnerabilities and ensure rapid reporting in the event of an emergency within the timeframes specified in the CRA.
Security as an Integral Part of Our Sensors
Cyber Resilience Act: Security as an Integral Part of Our Sensors

How Leuze supports CRA implementation

As a partner for secure sensor solutions, Leuze guides product users through the transition period until the CRA is fully implemented. The sensor manufacturer provides information on the requirements and shares best-practice approaches. Customers receive guidance on their questions regarding the CRA – from selecting suitable products to ensuring their safe integration into existing systems. Information services include:

  • Customized consultation: Experts are on hand to assist customers in evaluating their systems and components.
  • Application recommendations: Leuze provides specific guidance on how to operate sensors and control systems safely.
  • Documentation support: Customers receive assistance in preparing the necessary technical documentation.
  • Information on reporting procedures: Leuze explains how to report security incidents and what steps to take in the event of an emergency.

Download technology report
Senior-Experte Herbert Koebel
The author

Herbert Köbel
Senior Expert - R&D Software
Email: herbert.koebel@leuze.com
Web: www.leuze.com